The future of cabling

A lot of movies “predict” the future. While some come true, we are still waiting for somethings to happen. The one thing that will be consistent will be the cabling infrastructure because the data will need to travel from point to point. In this blog, Danny Cohen, an account manager at LINX, a member of the CommScope PartnerPRO Network, explains that the future will migrate from copper to fiber eventually.

19_future_cabling(Note: The following has been submitted as a guest post to CommScope Blogs by Danny Cohen, account manager at LINX. LINX is a member of CommScope’s PartnerPRO Network and provider of IT networking solutions in the United States. Opinions and comments provided in this guest post, as with all posts to CommScope Blogs, are that of the author and do not necessarily reflect the views of CommScope.)

It’s hard to imagine what the future will look like. 2001: A Space Odyssey didn’t get too many things right. I mean we didn’t even get the iPhone until 2007. Flying around space with an AI computer still seems far out, even on today’s standards. Stanley Kubrick took a risk in predicting the future of technology. Some things take off like mini computers that fit in my pocket and talking thermostat. Others seems to die before becoming real. It’s 2019, where is my flying car?

Technology trends in our personal life are now driving trends in the business world. If you don’t believe me, pull out your work-issued Blackberry and spend 10 minutes writing me an email about how you disagree. The Netflix Model, otherwise known as Software as a Service (SaaS), has changed the way we operate day-to-day business.

What will be the next technology trend that changes the way we do business? It’s easy to look at the next five years and say things like cloud, co-located data centers, and IoT (Internet of Things) will continue to drive changes. But what comes next?

CLICK TO TWEET: Danny Cohen from LINX tries to predict the future of cabling.

The short answer is no one knows. Businesses must look at the future and prepare for it. No one wants to be that company in 2013 to invest millions in a new onsite data center only to move to the cloud in 2014. Trust me, that happened (and is still happening). Businesses that are too short sided to look at future trends can end up spending way more in the long run.

Cabling is the infrastructure that supports business operations today and it will only continue to be more important. One thing is clear about the future of cabling, bandwidth requirements will only continue to go up. While some think cables will go away with wireless, they forget that those wireless units (access points) still need to be wired. So, while the cabling needs and designs will change, the importance of cabling will continue to grow.

Today’s best copper cable, Category 6a, can support 10 Gbps speed at 100 meters. That’s a lot. It’s crazy to think we’ll ever need more than that. On the other hand, in 1990 when Category 3 cable was created and supported 10 Mbps I’m sure we had the same thinking. We thought 10 Mbps was a fast speed back then. At the time, few devices would even support that much speed.

The main difference between Category 6a cable and Category 6 is the diameter. Category 6a essentially has more copper, thus increasing its capability. Category 7, which is not widely available yet, will be even thicker, filled with more copper to support even more distance and speed. At some point, we’re going to run into physical issues with using copper.

Now, in comes fiber optic cable. Unless you’re in the industry, you probably have to thank Google if you’ve heard of fiber. You probably have other things to thank Google for, but that’s for another blog. Fiber is made from thin strands of glass. Instead of sending a signal over copper, fiber sends bursts of light through the thin glass strand. This different cable construction allows for fiber to have much higher bandwidth and distance limitations compared to copper.

Today, we mainly use fiber for underground (outside plant) or backbone (riser) cable. One reason for this is cost. The cost of fiber has always been more than copper. That’s still the case today; however, the difference between the two is shrinking and has never been closer than it is today. The price will continue to fall as more of it get produced. At some point, cost won’t be a factor. The other factor in how fiber is used is the end devices. Today’s devices don’t directly support a fiber connection. Look on the back of your computer and see if there’s a fiber port. Since the end devices don’t connect to fiber directly, a copper conversion must happen at some point.

As cost continues to come down and more devices come out with a direct fiber connection, you’ll see the use of fiber cabling increase. Some wireless access points and security cameras take a direct fiber connection today, so it’s only a matter of time until that becomes the standard. Fiber can support speeds over 100 Gbps and has even been tested at a terabyte per second. That’s crazy speeds and again it’s hard to imagine needing all that.

As a low voltage contractor, a lot of our work is ripping and replacing old cable with new ones. Most just upgrade to the newest version of copper, knowing that we’ll be back out in a handful of years to do the same thing again. I encourage customers to look ahead and see if there is a better way to do this. While a fiber install today might cost a little more, it will save money in the long run. It doesn’t take a special company to take advantage of a fiber infrastructure, just a company that’s willing to ask, “is there a better way to do this”?