Ruckus Networks (now part of CommScope via acquisition) announced that its technology will be used in the Wi-Fi hotspots of Google Station in São Paulo. Ruckus will provide the devices and technologies needed to supply the carriers' networks in the Google Station hotspots. Among the technologies, Ruckus will provide its Virtual SmartZone Controller, Ruckus T310 outdoor Wi-Fi access points, and Ruckus R510 (higher density) and R310 (lower density) in indoor environments.
The project includes the replacement of 120 Wi-Fi points in operation in the state capital and the deployment of other 499 – totaling 619 access points available in the city of São Paulo, including locations such as Ibirapuera Park and CPTM train stations. All points in Brazil can be seen in the Google Station Map. The plan is to expand the service to millions of Brazilians by the end of 2020.
Google Station is a high-quality, high-speed public Wi-Fi platform that provides an easy set of Wi-Fi hotspot deployment tools in public and high-traffic locations, such as airports, shopping malls, universities, train stations and mass transit stations. These Wi-Fi hotspots provide high performance using BeamFlex™, Ruckus’ patented adaptive antenna technology, which ensures greater performance and connectivity, a better signal and maximum energy efficiency.
The promise is that the Internet is fast enough for the user to watch high quality videos on their mobile device without needing to spend their data plan. To connect, just find and select the "Google Station" network and enter your phone number. The confirmation will be made with a code sent via SMS.
"Deploying Google Station with Ruckus technologies is an important step in connecting the next billion users," said David Shapiro, Chief Business Officer of Google's Next Billion Users initiative. "Ruckus networks are simple to install and operationally cost-effective, allowing for a very rapid deployment. In addition, its robust Wi-Fi signal ensures constant connectivity with Google Station hotspots, so users can download/upload photos, manage points of sale, and stay connected without interruption."
"I consider this project an important milestone in the democratization of high-speed Internet access in Brazil,” said Marcos Dias, Regional Sales Director for Brazil at Ruckus Networks.
“We are talking about a no-charge service for the citizen that is literally raising the bar of user experience in Wi-Fi access. With this Ruckus solution, we are providing cutting-edge technologies such as BeamFlex, ChannelFly and PD-MRC which, in practice, mean better coverage with fewer antennas and more capacity to withstand a high density of users with a significant flow of data. That's just the beginning!"
Ruckus technologies are currently deployed in hundreds of Wi-Fi hotspots in Google Stations in India, Mexico, and Indonesia.
Follow Ruckus Networks on LinkedIn and Facebook in Portuguese to get the latest news.
—FIM—
Sobre a CommScope:
CommScope (NASDAQ: COMM) e as recém-adquiridas ARRIS e Ruckus Networks estão redefinindo o amanhã, moldando o futuro das comunicações com fio e wireless. Nossa equipe global combinada de funcionários, inovadores e tecnólogos permitem que clientes em todas as regiões do mundo antecipem o que vem pela frente e rompam os limites do que é possível. Descubra mais em www.commscope.com.
Siga nos no Twitter e LinkedIn e nos curta no Facebook.
Se inscreva para nossos press releases e posts de blogs.
Este comunicado à imprensa inclui declarações prospectivas baseadas em informações atualmente disponíveis para a administração, em crenças da administração e em várias suposições relacionadas a eventos futuros. As declarações prospectivas não são uma garantia de desempenho e estão sujeitas a uma série de incertezas e outros fatores, que podem fazer com que os resultados reais sejam materialmente diferentes dos atualmente esperados. Ao fornecer declarações prospectivas, a empresa não pretende, e não está assumindo nenhuma obrigação ou dever, atualizar essas declarações como resultado de novas informações, eventos futuros ou outros.
Fonte: CommScope
Contato com a mídia:
Kris Kozamchak, CommScope
+1-972-792-3311 or publicrelations@commscope.com
Contato financeiro:
Kevin Powers, CommScope
+1-828-323-4970